STM32H5 ADC Measuring VREF+
Good morning,
I would like to measure the supply voltage on an STM32H573RI. To do this, I measure VREFINT and then want to calculate the supply voltage.
My approach (simplified):
sConfig.Channel = ADC_CHANNEL_VREFINT;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_640CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
while (!__HAL_ADC_GET_FLAG(&hadc1, ADC_FLAG_EOC));
return HAL_ADC_GetValue(&hadc1);
Using the ADC value of VREFINT, I calculate the supply voltage as follows:
static uint16_t Calc_VREF(uint16_t adc_value)
{
uint16_t vrefint_cal = (uint16_t) (*(uint16_t *) (0x08FFF810));
uint16_t vrefint_voltage = 3300;
return (uint16_t)(vrefint_voltage * vrefint_cal / adc_value);
}
My ADC delivers a value of 1.562 digits for VREFINT, while the calibration value is 1.503 digits. According to my calculations, the reference voltage is therefore 3.175 V. However, VDD / VDDA/VREF+ / VBAT are at 3.358 V (VSS / VSSA/VREF- = GND).
This means that all measurements taken by the ADC are subject to error. Is there an explanation for why the measurements are so inaccurate? How can I ensure that I can obtain accurate measurements with the ADC?
Many thanks.
Andreas