STM32H5 JTDO/TRACESWO pin not working as UART7_RX despite alternate function support
Hi ST community,
I’m working with an STM32H563 MCU and trying to use the pin labeled JTDO/TRACESWO as UART7_RX because the datasheet/alternate function table shows that this pin supports UART7_RX.
However, UART transmission works correctly, but UART reception does not work when using this pin. If I switch to a different pin, both TX and RX function as expected.
Here’s what I’ve checked so far:
- Configured the pin in STM32CubeMX as UART7_RX (alternate function mode)
- Verified UART7 peripheral initialization is correct
- Checked baud rate and UART settings
- Confirmed hardware wiring:
- External TX connected to STM32 UART7_RX
- Common GND connected
- Signal level is 3.3V
- Tried disabling trace/SWO in CubeMX by setting by debug to “Serial Wire” instead of trace mode
- Also tested with debugger disconnected after programming
My question:
- Is the JTDO/TRACESWO pin fully usable as UART7_RX on STM32H5, or is it reserved/limited due to debug trace functionality?
- Is there any additional register/configuration needed to release this pin from SWO/JTAG?
- Has anyone successfully used this pin as UART RX in an STM32H5 project?
MCU part number: STM32H563RGT6
Package: LQFP64
Pin name: PB7/UART7_RX(55 num Pin)
Toolchain: STM32CubeMX / STM32CubeIDE
Debugger: ST-Link V2
Any guidance would be appreciated. Thanks!