Skip to main content
Visitor II
March 25, 2026
Question

STM32H5 VCORE drop detection

  • March 25, 2026
  • 1 reply
  • 163 views

Hello,

Is my understanding correct that it's impossible to internally detect short (<100ns) drops of VCORE internally?

Reading RM0481 page 154 it seems impossible to directly monitor VCORE through the tamper mechanism which I assume forces the use of an ADC+WDG, which probably puts the detection range in the µs? Which means the target is sensitive to fault injections?

1 reply

KDJEM.1
Technical Moderator
April 9, 2026

Hello @gquere and welcome to the community;

 

As mentioned in the datasheet the minimum TS_VCore is 1 µs, with ADC sampling time when reading the VCORE voltage. Note that the VCORE monitoring characteristics value is specified by design and not tested in production.

KDJEM1_0-1775746371241.png

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.