Skip to main content
Associate II
August 12, 2025
Solved

stm32h533re execute code in sram1

  • August 12, 2025
  • 1 reply
  • 364 views

Hello members,

Until recently, I was using a G473. There, I ran code from the ccmram. That worked without any problems. Now I have switched to the H533. For performance reasons, I want to run the code in SRAM1 0x20000000 - 0x2001FFF. I want to keep the data in SRAM2.

MEMORY
{
RAM (xrw) : ORIGIN = 0x20020000, LENGTH = 80K /*Ram placed SRAM2 with ECC-Check*/
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 256K
CCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K /*SRAM1 for code */
}

For example, the function:

__attribute__((section(“.ccmram”))) void EXTI0_IRQHandler();


is located in the map file at the correct address:

.text.EXTI0_IRQHandler
0x0000000020000300 0x28 ./Hal/Interface/Interrupts.o
0x0000000020000300 EXTI0_IRQHandler

The code is copied to SRAM1 in the startup file.

However, when I call the function, a hard fault is generated.
The PC points to the address: 0x20000302
The CFSR register contains: 0x01000000, which
corresponds to UFSR[8] and means unaligned access. This would match the pc address: 0x20000302.

Now my question: Is there an easy way to allow unaligned access in SRAM1? For example, by configuring the MPU or by remapping SRAM1 to 0x10000000, for example. In my research so far, I have not found a solution that works for me.
(I am using CubeIde with gcc)

Thanks in advance

jhoerd

 

Best answer by jhoerd

Hello NesrynELMK,

Thank you very much for your reply. I am only responding now because I did not know how to describe my problem more specifically.
I was already familiar with the example you mentioned. However, it does not apply to my specific use case or problem. While trying to describe my problem better, I came up with the solution.

I am using CubeIde with gcc and SRAM2 for data and SRAM1 for code.

Two fundamental problems arose in my example.
1. Alignment of static, global variables
When calling:
/* Call static constructors */
bl __libc_init_array
in StartupFile.s, a hard fault occurred. This error was due to alignment in the memory area for few global static variables.
This was resolved by using the aligned(4) attribute.
__attribute__(( aligned(4))) type1 variable1;

2. alignment von code in sram1
I place vector table and code in sram1 using the following linker instruction:

_sivector = LOADADDR(.isr_vector);

.isr_vector :

{

. = ALIGN(4);

KEEP(*(.isr_vector)) /* Startup code */

. = ALIGN(4);

} >CODERAM AT>FLASH

.coderam :

{

. = ALIGN(4);

_scoderam = .;

*(.coderam)

*(.coderam*)

*/sampleFile.o(.text .text*)

. = ALIGN(4);

_ecoderam = .;

} >CODERAM AT>FLASH

A bus fault was triggered during the execution of the code. While investigating the error, I noticed the following in the linker map file:

*(.isr_vector)
.isr_vector 0x0000000020000000 0x254 ./startupH523x.o
0x0000000020000000 g_pfnVectors
0x0000000020000254 . = ALIGN (0x4)

.coderam 0x0000000020000258 0xef8 load address 0x0000000008000254
0x0000000020000258 . = ALIGN (0x4)
0x0000000020000258 _scoderam = .

//content

//at end of codeRam area:

0x0000000020001090 0xc0 linker stubs
0x0000000020001150 . = ALIGN (0x4)
0x0000000020001150 _ecoderam = .
0x000000000800114c _sidata = LOADADDR (.data)

The offset of -4 at the end and +4 at the beginning of the codram area seemed suspicious to me.

I changed the alignment specification in the linker script as follows:

_sivector = LOADADDR(.isr_vector);

.isr_vector :

{

. = ALIGN(4);

KEEP(*(.isr_vector)) /* Startup code */

. = ALIGN(8);

} >CODERAM AT>FLASH

.coderam :

{

. = ALIGN(8);

_scoderam = .;

*(.coderam)

*(.coderam*)

*/sampleFile.o(.text .text*)

. = ALIGN(8);

_ecoderam = .;

} >CODERAM AT>FLASH

This removed the offset from the map file.

.isr_vector 0x0000000020000000 0x254 ./startupH523x.o
0x0000000020000000 g_pfnVectors
0x0000000020000258 . = ALIGN (0x8)
*fill* 0x0000000020000254 0x4

.coderam 0x0000000020000258 0xef8 load address 0x0000000008000258
0x0000000020000258 . = ALIGN (0x8)
0x0000000020000258 _scoderam = .

//at end of codeRam area:

0x0000000020001090 0xc0 linker stubs
0x0000000020001150 . = ALIGN (0x8)
0x0000000020001150 _ecoderam = .
0x0000000008001150 _sidata = LOADADDR (.data)

This means that my code now also works in the SRAM area without any problems.

Perhaps my insight will also help others who have a similar problem.

How do I mark the thread as resolved?
Thanks again for your help.

best regards

jhoerd

1 reply

ST Employee
August 13, 2025

Hello @jhoerd 

Please take a look at this article: https://community.st.com/t5/stm32-mcus/how-to-place-and-execute-stm32-code-in-sram-memory-with/ta-p/49528

It provides a detailed explanation on how to execute the entire firmware directly from embedded SRAM memory.

 

 

Kind regards,

jhoerdAuthorBest answer
Associate II
September 8, 2025

Hello NesrynELMK,

Thank you very much for your reply. I am only responding now because I did not know how to describe my problem more specifically.
I was already familiar with the example you mentioned. However, it does not apply to my specific use case or problem. While trying to describe my problem better, I came up with the solution.

I am using CubeIde with gcc and SRAM2 for data and SRAM1 for code.

Two fundamental problems arose in my example.
1. Alignment of static, global variables
When calling:
/* Call static constructors */
bl __libc_init_array
in StartupFile.s, a hard fault occurred. This error was due to alignment in the memory area for few global static variables.
This was resolved by using the aligned(4) attribute.
__attribute__(( aligned(4))) type1 variable1;

2. alignment von code in sram1
I place vector table and code in sram1 using the following linker instruction:

_sivector = LOADADDR(.isr_vector);

.isr_vector :

{

. = ALIGN(4);

KEEP(*(.isr_vector)) /* Startup code */

. = ALIGN(4);

} >CODERAM AT>FLASH

.coderam :

{

. = ALIGN(4);

_scoderam = .;

*(.coderam)

*(.coderam*)

*/sampleFile.o(.text .text*)

. = ALIGN(4);

_ecoderam = .;

} >CODERAM AT>FLASH

A bus fault was triggered during the execution of the code. While investigating the error, I noticed the following in the linker map file:

*(.isr_vector)
.isr_vector 0x0000000020000000 0x254 ./startupH523x.o
0x0000000020000000 g_pfnVectors
0x0000000020000254 . = ALIGN (0x4)

.coderam 0x0000000020000258 0xef8 load address 0x0000000008000254
0x0000000020000258 . = ALIGN (0x4)
0x0000000020000258 _scoderam = .

//content

//at end of codeRam area:

0x0000000020001090 0xc0 linker stubs
0x0000000020001150 . = ALIGN (0x4)
0x0000000020001150 _ecoderam = .
0x000000000800114c _sidata = LOADADDR (.data)

The offset of -4 at the end and +4 at the beginning of the codram area seemed suspicious to me.

I changed the alignment specification in the linker script as follows:

_sivector = LOADADDR(.isr_vector);

.isr_vector :

{

. = ALIGN(4);

KEEP(*(.isr_vector)) /* Startup code */

. = ALIGN(8);

} >CODERAM AT>FLASH

.coderam :

{

. = ALIGN(8);

_scoderam = .;

*(.coderam)

*(.coderam*)

*/sampleFile.o(.text .text*)

. = ALIGN(8);

_ecoderam = .;

} >CODERAM AT>FLASH

This removed the offset from the map file.

.isr_vector 0x0000000020000000 0x254 ./startupH523x.o
0x0000000020000000 g_pfnVectors
0x0000000020000258 . = ALIGN (0x8)
*fill* 0x0000000020000254 0x4

.coderam 0x0000000020000258 0xef8 load address 0x0000000008000258
0x0000000020000258 . = ALIGN (0x8)
0x0000000020000258 _scoderam = .

//at end of codeRam area:

0x0000000020001090 0xc0 linker stubs
0x0000000020001150 . = ALIGN (0x8)
0x0000000020001150 _ecoderam = .
0x0000000008001150 _sidata = LOADADDR (.data)

This means that my code now also works in the SRAM area without any problems.

Perhaps my insight will also help others who have a similar problem.

How do I mark the thread as resolved?
Thanks again for your help.

best regards

jhoerd