Solved
STM32H562/3: clarify the max frequencies in DS14258 rev6
- January 5, 2026
- 1 reply
- 383 views
- According to the STM32 datasheet, the maximum clock frequency of TIM6 and TIM17 is shown as 64 MHz, while that of TIM1 to TIM8 is shown as 200 MHz. There is a conflict in the documentation, so please confirm which one is correct. (DS14258 Rev6,page 132)
- The datasheet indicates that the maximum supported clock frequency of SPI is 100 MHz, but no errors are displayed when configuring 200 MHz in CubeMX. Please confirm the actual maximum clock frequency of SPI.