Question
STM32H563 Nucleo Failed to execute a image in Flash using USART Bootloader Go command
Hi,
On the STM32H563 Nucleo, I was able to flash an application using the UART bootloader.
However, the application does not execute when triggered with the GO command.
If BOOT0 is pulled low, the same firmware runs successfully.
But Go command executes properly but the firmware is not running
The firmware i am trying is led blinking application