Skip to main content
Associate II
August 7, 2025
Question

STM32H573 SDMMC NEGEDGE valid/hold time

  • August 7, 2025
  • 0 replies
  • 264 views

Dear ST Community,

I am using the STM32H573's SDMMC interface to communicate with a soft eMMC device implemented in FPGA:

  • 1.8V I/O
  • DDR==0 mode
  • CLKDIV>0.

I'm setting up the timing constraints for the FPGA's CMD input versus the CK input and I have a query about the SDMMC interface timing.

In the datasheet, Table 123 defines the tov and toh parameters. In which mode are these parameters valid? CLKDIV>0 and NEGEDGE==0?

How would NEGEDGE==1 change tov and toh? Based on the diagrams of figure 164, I believe the tov and toh would increase by 1/2 the clock period. Is that correct?

Thank you. Ben