Skip to main content
Associate
September 30, 2025
Question

STM32H723VGT6 hardware error interrupt is occurring

  • September 30, 2025
  • 1 reply
  • 528 views

hi ;During the operation of STM32H723VGT6, the constant input bus error and hardware error interrupt occurred, and the clock is 280M. The PWR_REGULATOR_VOLTAGE_SCALE1 is unstable. The clock configuration __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0) was modified. The result is stable. Could you please help confirm what the reason isst ..................jpg

1 reply

STOne-32
Technical Moderator
September 30, 2025

Dear @leo12345678 ,

can you let us know which clock is at 280MHz , CPU one of AXI Bus or AHB ?

IMG_4500.jpeg

A special care also to check with pins 48 and 73 that are connected to VCAP capacitor of 2.2uF having a Lower value may create such behavior .

Hope it helps you .

STOne-32