Skip to main content
Associate III
August 22, 2025
Solved

[STM32H743XGH6] Flash memory

  • August 22, 2025
  • 1 reply
  • 207 views

I believe the STM32H743XGH6 has 1 MB of internal flash memory. However, using STM32CubeProgrammer, I was able to write and read data to the reserved area at 0x8180 0000. Is it okay to use this area?

The built-in Flash Memory areas of the STM32H743XGH6 are recognized as
0x8100 0000-0x817F FFFF and 0x8000 0000-0x0801 FFFF.

Best answer by mƎALLEm

Hello,

This zone of Flash is physically available but not tested in production so its usage is not guaranteed: its usage is  NOT recommended.

1 reply

mƎALLEm
mƎALLEmBest answer
Technical Moderator
August 22, 2025

Hello,

This zone of Flash is physically available but not tested in production so its usage is not guaranteed: its usage is  NOT recommended.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."