Skip to main content
Associate II
July 8, 2025
Question

STM32H753VI thermal dissipation calculation

  • July 8, 2025
  • 1 reply
  • 253 views

Hi Team,

 

We are performing thermal simulation where the part STM32H753VI included in my board.

We are powering STM with 3V3 and we would like to understand the below parameters,

1)Tj,

2)Thermal simulation data if any

3) Efficiency to calculate the power dissipation?

 

Also, we could see some document An5036: section 6.1.1,table 4: we would like to understand how you calculated the dissipation values? Note: we aware the document is for different STM from ours.

 

Your prompt support on this will be highly appreciated !

Regards,
Manikandan R.

1 reply

ELABI.1
Technical Moderator
July 8, 2025

Hi @Manikandan,

For your first question, the term Tj refers to the junction temperature, which is the maximum internal temperature that the core of the microcontroller can reach during operation. It is calculated as follows:

TJ max = TA max + (PD max × ΘJA)

For your third question, power dissipation is the amount of electrical energy converted into heat. This dissipation is important because it affects the internal temperature and is calculated as follows:

PI/O max = Σ (VOL × IOL) + Σ((VDD – VOH) × IOH)

You can refer to the STM32H753 Datasheet, specifically section 8.10 "Thermal Characteristics," where these formulas are well explained:

 

ELABI1_1-1751983814474.png

But for question 2) Thermal simulation data if any, I don't understand your question, could you please explain it to me in more detail?

Thanks.

ELABI.1

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.