STM32H755 HRTIM and USB multiplexing
Hello everyone,
I am using the NUCLEO-H755ZI-Q board for a project. I have noticed that the HRTIMs that
are not multiplexed with some USB pins (like the HRTIM_D1 with the D+ for programming the IC via usb)
work normally, while if they do, I can't output any PWM pulse. Is this actually a thing and to overcome it
I have to remove some of the Zero Ohm resistors behind the nucleo board or design a custom pcb for my needs
or am I messing something up? In my situation specifically, i can output from all HRTIM channels except the D1
and D2, both of which map to a pin with USB.
Thanks in advance!