STM32H757: TDM slots and bit depth over SAI interface
I'm working on a device that requires requires 12 audio output channels and 10 input channels. I wish to do this over 16-slot TDM. Now, I'm concerned about whether this can be done with 32 bits per sample. The reference manual states in section 54.4.6 Frame synchronization "The audio frame length can be configured to up to 256 bit clock cycles". 256/16=16. Does this mean I can only do 16-bit audio with 16-slot TDM? Or did I misread.