STM32H7R7: How to setup memory mapped XSPI for external HyperRAM S70KL1282?
Hi,
we are using the STM32H7R7I8T6 MCU with an Infineon S70KL1282 HyperRAM Chip attached on XSPI1 and configured via CubeMX, we are looking for an example for the correct timing/parameters to use the RAM Chip in memory mapped mode as Graphics RAM.
Our current config makes makes reading and writing possible but the memory contains garbarge data.
We are repeatedly trying to write the string "1234567890" into the external RAM but we get back the following:

The current config is built from various other examples we could find like this one: https://github.com/STMicroelectronics/STM32CubeH7/blob/master/Projects/STM32H735G-DK/Examples/OSPI/OSPI_HyperRAM_MemoryMapped/Src/main.c but the parameters do not match exactly.
Our current code looks like this:
/**
* @brief XSPI1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_XSPI1_Init(void)
{
/* USER CODE BEGIN XSPI1_Init 0 */
/* USER CODE END XSPI1_Init 0 */
XSPIM_CfgTypeDef sXspiManagerCfg = {0};
XSPI_HyperbusCfgTypeDef sHyperBusCfg = {0};
/* USER CODE BEGIN XSPI1_Init 1 */
hxspi1.Instance = XSPI1;
HAL_XSPI_DeInit(&hxspi1);
/* USER CODE END XSPI1_Init 1 */
/* XSPI1 parameter configuration*/
hxspi1.Instance = XSPI1;
hxspi1.Init.FifoThresholdByte = 4;
hxspi1.Init.MemoryMode = HAL_XSPI_SINGLE_MEM;
hxspi1.Init.MemoryType = HAL_XSPI_MEMTYPE_HYPERBUS;
hxspi1.Init.MemorySize = HAL_XSPI_SIZE_128MB;
hxspi1.Init.ChipSelectHighTimeCycle = 8;
hxspi1.Init.FreeRunningClock = HAL_XSPI_FREERUNCLK_DISABLE;
hxspi1.Init.ClockMode = HAL_XSPI_CLOCK_MODE_0;
hxspi1.Init.WrapSize = HAL_XSPI_WRAP_NOT_SUPPORTED;
hxspi1.Init.ClockPrescaler = 8;
hxspi1.Init.SampleShifting = HAL_XSPI_SAMPLE_SHIFT_NONE;
hxspi1.Init.ChipSelectBoundary = HAL_XSPI_BONDARYOF_64MB;
hxspi1.Init.MaxTran = 0;
hxspi1.Init.Refresh = 250;
hxspi1.Init.MemorySelect = HAL_XSPI_CSSEL_NCS1;
if (HAL_XSPI_Init(&hxspi1) != HAL_OK)
{
Error_Handler();
}
sXspiManagerCfg.nCSOverride = HAL_XSPI_CSSEL_OVR_NCS1;
sXspiManagerCfg.IOPort = HAL_XSPIM_IOPORT_1;
sXspiManagerCfg.Req2AckTime = 1;
if (HAL_XSPIM_Config(&hxspi1, &sXspiManagerCfg, HAL_XSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
sHyperBusCfg.RWRecoveryTimeCycle = 7;
sHyperBusCfg.AccessTimeCycle = 4;
sHyperBusCfg.WriteZeroLatency = HAL_XSPI_LATENCY_ON_WRITE;
sHyperBusCfg.LatencyMode = HAL_XSPI_FIXED_LATENCY;
if (HAL_XSPI_HyperbusCfg(&hxspi1, &sHyperBusCfg, HAL_XSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN XSPI1_Init 2 */
/* USER CODE END XSPI1_Init 2 */
}/* USER CODE BEGIN 4 */
/* This function enables memory-mapped mode for Read and Write operations */
void EnableMemMapped(void)
{
XSPI_HyperbusCmdTypeDef sCommand;
sCommand.AddressSpace = HAL_XSPI_MEMORY_ADDRESS_SPACE;
sCommand.AddressWidth = HAL_XSPI_ADDRESS_32_BITS;
sCommand.DQSMode = HAL_XSPI_DQS_ENABLE;
sCommand.Address = 0;
sCommand.DataLength = 1;
if(HAL_XSPI_HyperbusCmd(&hxspi1, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
XSPI_MemoryMappedTypeDef sMemMappedCfg;
sMemMappedCfg.TimeOutActivation = HAL_XSPI_TIMEOUT_COUNTER_DISABLE;
if(HAL_XSPI_MemoryMapped(&hxspi1, &sMemMappedCfg) != HAL_OK)
{
Error_Handler();
}
uint32_t address = 0;
uint16_t index1;/*index1 counter of bytes used when reading/
writing 256 bytes buffer */
uint16_t index2;/*index2 counter of 256 bytes buffer used when reading/
writing the 1Mbytes extended buffer */
mem_addr = (__IO uint8_t *)(XSPI1_BASE + address);
/*Writing 1Mbyte (256Byte BUFFERSIZE x 4096 times) */
for (index2 = 0; index2 < 4096; index2++)
{
for (index1 = 0; index1 < BUFFERSIZE; index1++)
{
*mem_addr = aTxBuffer[index1];
mem_addr++;
// HAL_GPIO_TogglePin(GPION, GPIO_PIN_4);
HAL_Delay(1); /* add delay to better see the toggling on the led when writing the PSRAM */
}
}
/*----------------------------------------------------------------------*/
/* Reading Sequence of 1Mbyte */
mem_addr = (__IO uint8_t *)(XSPI1_BASE + address);
/*Reading 1Mbyte (256Byte BUFFERSIZE x 4096 times)*/
for (index2 = 0; index2 < 4096; index2++) {
for (index1 = 0; index1 < BUFFERSIZE; index1++)
{
if (*mem_addr != aTxBuffer[index1])
{
HAL_GPIO_TogglePin(GPION, GPIO_PIN_4);
/*if data read is corrupted we can toggle a led here: example blue led*/
}
//HAL_GPIO_TogglePin(GPION, GPIO_PIN_4);
//HAL_Delay(1);
mem_addr++;
}
}
mem_addr = (__IO uint8_t *)(XSPI1_BASE + address);
HAL_GPIO_WritePin(GPION, GPIO_PIN_4, GPIO_PIN_RESET);
}
/*----------------------------------------------------------------------*/
/*This function is used to calibrate the Delayblock before initiating
USER's application read/write transactions*/
/* USER CODE END 4 */
Any help is very appreciated.