Skip to main content
Associate
August 19, 2025
Question

STM32H7S3L8 USB core reset timeout

  • August 19, 2025
  • 2 replies
  • 449 views

Hey, we have purchased the Nucleo board H7S3L8-B02. We always run in a timeout during USB core reset. This problem seems quite popular with multiple forum posts. However we still didn't manage to get it to run. I will give a set by step explanation of what we've done. Maybe someone catches the mistake. We made all of our settings in "Application", none in "Boot".

  • USB_OTG_FS settings:USB_OTG_FSUSB_OTG_FS
  • Middleware CDC settings:

 

 

CDCCDC

 

  • Power settings:PWRPWR

     

  • Clock settings (automatic by IDE)

CLKCLK

  • main.c:
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "usb_device.h"


/* Private function prototypes -----------------------------------------------*/
static void MPU_Config(void);
static void MX_GPIO_Init(void);


int main(void)
{

 MPU_Config();

 /* Update SystemCoreClock variable according to RCC registers values. */
 SystemCoreClockUpdate();

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USB_DEVICE_Init();

 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

static void MX_GPIO_Init(void)
{
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOM_CLK_ENABLE();
}


 /* MPU Configuration */
static void MPU_Config(void)
{
 MPU_Region_InitTypeDef MPU_InitStruct = {0};

 /* Disables the MPU */
 HAL_MPU_Disable();

 /* Disables all MPU regions */
 for(uint8_t i=0; i<__MPU_REGIONCOUNT; i++)
 {
 HAL_MPU_DisableRegion(i);
 }

 /** Initializes and configures the Region and the memory to be protected
 */
 MPU_InitStruct.Enable = MPU_REGION_ENABLE;
 MPU_InitStruct.Number = MPU_REGION_NUMBER0;
 MPU_InitStruct.BaseAddress = 0x0;
 MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
 MPU_InitStruct.SubRegionDisable = 0x87;
 MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
 MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
 MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
 MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
 MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
 MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

 HAL_MPU_ConfigRegion(&MPU_InitStruct);
 /* Enables the MPU */
 HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

void Error_Handler(void)
{
 __disable_irq();
 while (1)
 {
 }
}
#ifdef USE_FULL_ASSERT

void assert_failed(uint8_t *file, uint32_t line)
{

}
#endif /* USE_FULL_ASSERT */

 

 _hal_msp.c

/* Includes ------------------------------------------------------------------*/
#include "main.h"

void HAL_MspInit(void)
{

 PWR_PVDTypeDef sConfigPVD = {0};

 /* System interrupt init*/

 /** PVD Configuration
 */
 sConfigPVD.PVDLevel = PWR_PVDLEVEL_1;
 sConfigPVD.Mode = PWR_PVD_MODE_NORMAL;
 HAL_PWR_ConfigPVD(&sConfigPVD);

 /** Enable the PVD Output
 */
 HAL_PWR_EnablePVD();

 /* Enable USB Voltage detector */
 if(HAL_PWREx_EnableUSBVoltageDetector() != HAL_OK)
 {
 /* Initialization error */
 Error_Handler();
 }

 HAL_PWREx_EnableUSBReg();
}
  • usbd_conf.c
void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 if(pcdHandle->Instance==USB_OTG_FS)
 {
 /* USER CODE BEGIN USB_OTG_FS_MspInit 0 */

 /* USER CODE END USB_OTG_FS_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USBOTGFS;
 PeriphClkInit.UsbOtgFsClockSelection = RCC_USBOTGFSCLKSOURCE_HSI48;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }

 /** Enable USB Voltage detector
 */
 HAL_PWREx_EnableUSBVoltageDetector();

 __HAL_RCC_GPIOM_CLK_ENABLE();
 /**USB_OTG_FS GPIO Configuration
 PM14 ------> USB_OTG_FS_VBUS
 */
 GPIO_InitStruct.Pin = GPIO_PIN_14;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOM, &GPIO_InitStruct);

 /* Peripheral clock enable */
 __HAL_RCC_USB_OTG_FS_CLK_ENABLE();
 __HAL_RCC_USBPHYC_CLK_ENABLE();

 /* Peripheral interrupt init */
 HAL_NVIC_SetPriority(OTG_FS_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(OTG_FS_IRQn);
 /* USER CODE BEGIN USB_OTG_FS_MspInit 1 */

 /* USER CODE END USB_OTG_FS_MspInit 1 */
 }
}

 

  • problem:
static HAL_StatusTypeDef USB_CoreReset(USB_OTG_GlobalTypeDef *USBx)
{
 __IO uint32_t count = 0U;

 /* Wait for AHB master IDLE state. */
 do
 {
 count++;

 if (count > HAL_USB_TIMEOUT)
 {
 return HAL_TIMEOUT;
 }
 } while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_AHBIDL) == 0U);

 /* Core Soft Reset */
 count = 0U;
 USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST;

 do
 {
 count++;

 if (count > HAL_USB_TIMEOUT)
 {
 return HAL_TIMEOUT;
 }
 } while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST) == USB_OTG_GRSTCTL_CSRST);

 return HAL_OK;
}

2 replies

Technical Moderator
August 21, 2025

Hi @STesil 

Did you compare your configuration and setup with the provided examples. Also this article FAQ: Troubleshooting a USB core soft reset stuck could be helpful.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Technical Moderator
September 1, 2025

Hi @STesil 

Any update regarding the issue? Did you follow up the provided example firmware check USB cables?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL