Skip to main content
Visitor II
December 3, 2025
Question

STM32L031K6U6 - ADC Channel 9 Pin Mapping Clarification

  • December 3, 2025
  • 2 replies
  • 101 views

Hello ST Support Team,

I'm working with the STM32L031K6U6 (32-pin UFQFPN package) and need clarification on ADC channel mapping.

Question: Is there an ADC Channel 9 available on the STM32L031K6U6, and if so, which physical pin does it map to?

Context:
- I'm trying to use PB1 as an ADC input
- Documentation suggests ADC Channel 9 should be available

Could you please confirm:
1. Which pins have ADC capability on STM32L031K6U6 32-pin package?
2. Is ADC Channel 9 available on this specific package variant?
3. If ADC Channel 9 exists, which physical pin does it connect to?

Hardware: STM32L031K6U6 (32-pin UFQFPN package)
IDE: STM32CubeIDE
HAL Version: Latest

Thank you for your assistance.

2 replies

Technical Moderator
December 3, 2025

hello @vardhaman_k 
and welcome to ST community!
Based on the product Datasheet, Table 15, the ADC channel 9 pin is available on PB1.
Hope that helps
Gyessine

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TDK
Super User
December 3, 2025

CubeMX can highlight pins for you. This information is also available in the datasheet.

Here are the 10 pins with ADC capability on this chip:

TDK_0-1764772214681.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."