Skip to main content
Visitor II
March 16, 2026
Question

STM32L071 Operation Failure and Power Line Resistance

  • March 16, 2026
  • 2 replies
  • 144 views

Hello.
I recently experienced an unusual MCU Problem and need to analyze it. Please help me.

 

The FW program download to the MCU is successful, but it does not operate after a reset.

 

I performed a short circuit test after disconnecting the power(Battery)

but even when measuring VCC-GND and GND-VCC at the power supply, a resistance value of approximately 500 ohms is detected.

 

When I disconnect only the MCU from the PCB and re-measure, the 500 ohm value disappears from the PCB

but this value persists when measuring directly from the MCU pins.

 

Can I conclude that the MCU is dead due to a power supply failure?

And in what cases does this problem occur?

2 replies

mƎALLEm
Technical Moderator
March 16, 2026

Hello @JinMoon and welcome to the ST community,


@JinMoon wrote:

but even when measuring VCC-GND and GND-VCC at the power supply,


Do you mean VDD-GND? the power supply pins of the MCU?

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
TDK
Super User
March 16, 2026

500 ohms is lower than it should be and indicates damage. Damage typically results from an overvoltage condition.

But if it still connected and programmed, the application is likely running with an increase current draw.

"If you feel a post has answered your question, please click ""Accept as Solution""."