Skip to main content
Senior II
July 6, 2025
Question

STM32L433RC - Confusion with pin out with/without external SMPS

  • July 6, 2025
  • 2 replies
  • 258 views

I am designing a PCB that uses the STM32L433RC.

I just checked the pin out of the PCB footprint with the datasheet, but then got confused as there are two different pin outs for what seems to be the same device.

The footprint I am using matches figure 9 of the datasheet, not figure 8 (although I am not using the external SMPS).

The difference starts with pin 25 as shown in the diagrams below.

How is the pin out different for the same device ? Is this a setting in STM32CubeIDE ?

freeflyer_0-1751834022756.png

 

freeflyer_0-1751834195465.png

 

 

2 replies

AScha.3
Super User
July 6, 2025

Its same chip, but different version: with smps or not .

see ds :

AScha3_0-1751835565418.png

AScha3_1-1751835714198.png

 

 

- so decide, what you want .

see mouser: has also a P version :

https://www.mouser.de/c/semiconductors/embedded-processors-controllers/microcontrollers-mcu/arm-microcontrollers-mcu/?m=STMicroelectronics&series=STM32L433RC

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Super User
July 6, 2025

As @AScha.3 says, the SMPS version has a different part number with "P" appended. Similar part, but pinout is different as you saw and it has a different part number.

TDK_0-1751842843336.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."