Skip to main content
Associate
July 7, 2025
Solved

STM32L471 ADC maximum sampling rate

  • July 7, 2025
  • 1 reply
  • 380 views

I have the following clock tree for STM32L471

kasarghu_0-1751879106670.png

I am using TIM2 as trigger for DAC, ADC1, and ADC2 at 2.4MHz. Clock frequency of TIM2 is 48MHz with a counter value of 19 and prescaler = 0.

With oscilloscope, I confirmed that the DAC is generating the signal at 2.4MHz sampling frequency.

The ADC1 and ADC2 are running in dual mode with single DMA channel. The following is the ADC configuration

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file adc.c
 * @brief This file provides code for the configuration
 * of the ADC instances.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "adc.h"

/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

ADC_HandleTypeDef hadc1;
ADC_HandleTypeDef hadc2;
ADC_HandleTypeDef hadc3;
DMA_HandleTypeDef hdma_adc1;

/* ADC1 init function */
void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = ENABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T2_TRGO;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_DUALMODE_REGSIMULT;
 multimode.DMAAccessMode = ADC_DMAACCESSMODE_12_10_BITS;
 multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_1CYCLE;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_DIFFERENTIAL_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}
/* ADC2 init function */
void MX_ADC2_Init(void)
{

 /* USER CODE BEGIN ADC2_Init 0 */

 /* USER CODE END ADC2_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC2_Init 1 */

 /* USER CODE END ADC2_Init 1 */

 /** Common config
 */
 hadc2.Instance = ADC2;
 hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
 hadc2.Init.Resolution = ADC_RESOLUTION_12B;
 hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc2.Init.LowPowerAutoWait = ENABLE;
 hadc2.Init.ContinuousConvMode = DISABLE;
 hadc2.Init.NbrOfConversion = 1;
 hadc2.Init.DiscontinuousConvMode = DISABLE;
 hadc2.Init.DMAContinuousRequests = DISABLE;
 hadc2.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc2.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_DIFFERENTIAL_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC2_Init 2 */

 /* USER CODE END ADC2_Init 2 */

}
/* ADC3 init function */
void MX_ADC3_Init(void)
{

 /* USER CODE BEGIN ADC3_Init 0 */

 /* USER CODE END ADC3_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC3_Init 1 */

 /* USER CODE END ADC3_Init 1 */

 /** Common config
 */
 hadc3.Instance = ADC3;
 hadc3.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
 hadc3.Init.Resolution = ADC_RESOLUTION_12B;
 hadc3.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc3.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc3.Init.LowPowerAutoWait = DISABLE;
 hadc3.Init.ContinuousConvMode = DISABLE;
 hadc3.Init.NbrOfConversion = 1;
 hadc3.Init.DiscontinuousConvMode = DISABLE;
 hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc3.Init.DMAContinuousRequests = DISABLE;
 hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc3.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc3) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC3_Init 2 */

 /* USER CODE END ADC3_Init 2 */

}

static uint32_t HAL_RCC_ADC_CLK_ENABLED=0;

void HAL_ADC_MspInit(ADC_HandleTypeDef* adcHandle)
{

 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(adcHandle->Instance==ADC1)
 {
 /* USER CODE BEGIN ADC1_MspInit 0 */

 /* USER CODE END ADC1_MspInit 0 */
 /* ADC1 clock enable */
 HAL_RCC_ADC_CLK_ENABLED++;
 if(HAL_RCC_ADC_CLK_ENABLED==1){
 __HAL_RCC_ADC_CLK_ENABLE();
 }

 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**ADC1 GPIO Configuration
 PC0 ------> ADC1_IN1
 PC1 ------> ADC1_IN2
 PA2 ------> ADC1_IN7
 */
 GPIO_InitStruct.Pin = V_DUT_P_Pin|V_DUT_N_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG_ADC_CONTROL;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = GPIO_PIN_2;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG_ADC_CONTROL;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /* ADC1 DMA Init */
 /* ADC1 Init */
 hdma_adc1.Instance = DMA1_Channel1;
 hdma_adc1.Init.Request = DMA_REQUEST_0;
 hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
 hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
 hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
 hdma_adc1.Init.Mode = DMA_NORMAL;
 hdma_adc1.Init.Priority = DMA_PRIORITY_LOW;
 if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_LINKDMA(adcHandle,DMA_Handle,hdma_adc1);

 /* USER CODE BEGIN ADC1_MspInit 1 */

 /* USER CODE END ADC1_MspInit 1 */
 }
 else if(adcHandle->Instance==ADC2)
 {
 /* USER CODE BEGIN ADC2_MspInit 0 */

 /* USER CODE END ADC2_MspInit 0 */
 /* ADC2 clock enable */
 HAL_RCC_ADC_CLK_ENABLED++;
 if(HAL_RCC_ADC_CLK_ENABLED==1){
 __HAL_RCC_ADC_CLK_ENABLE();
 }

 __HAL_RCC_GPIOC_CLK_ENABLE();
 /**ADC2 GPIO Configuration
 PC2 ------> ADC2_IN3
 PC3 ------> ADC2_IN4
 */
 GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG_ADC_CONTROL;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /* USER CODE BEGIN ADC2_MspInit 1 */

 /* USER CODE END ADC2_MspInit 1 */
 }
 else if(adcHandle->Instance==ADC3)
 {
 /* USER CODE BEGIN ADC3_MspInit 0 */

 /* USER CODE END ADC3_MspInit 0 */
 /* ADC3 clock enable */
 HAL_RCC_ADC_CLK_ENABLED++;
 if(HAL_RCC_ADC_CLK_ENABLED==1){
 __HAL_RCC_ADC_CLK_ENABLE();
 }
 /* USER CODE BEGIN ADC3_MspInit 1 */

 /* USER CODE END ADC3_MspInit 1 */
 }
}

void HAL_ADC_MspDeInit(ADC_HandleTypeDef* adcHandle)
{

 if(adcHandle->Instance==ADC1)
 {
 /* USER CODE BEGIN ADC1_MspDeInit 0 */

 /* USER CODE END ADC1_MspDeInit 0 */
 /* Peripheral clock disable */
 HAL_RCC_ADC_CLK_ENABLED--;
 if(HAL_RCC_ADC_CLK_ENABLED==0){
 __HAL_RCC_ADC_CLK_DISABLE();
 }

 /**ADC1 GPIO Configuration
 PC0 ------> ADC1_IN1
 PC1 ------> ADC1_IN2
 PA2 ------> ADC1_IN7
 */
 HAL_GPIO_DeInit(GPIOC, V_DUT_P_Pin|V_DUT_N_Pin);

 HAL_GPIO_DeInit(GPIOA, GPIO_PIN_2);

 /* ADC1 DMA DeInit */
 HAL_DMA_DeInit(adcHandle->DMA_Handle);
 /* USER CODE BEGIN ADC1_MspDeInit 1 */

 /* USER CODE END ADC1_MspDeInit 1 */
 }
 else if(adcHandle->Instance==ADC2)
 {
 /* USER CODE BEGIN ADC2_MspDeInit 0 */

 /* USER CODE END ADC2_MspDeInit 0 */
 /* Peripheral clock disable */
 HAL_RCC_ADC_CLK_ENABLED--;
 if(HAL_RCC_ADC_CLK_ENABLED==0){
 __HAL_RCC_ADC_CLK_DISABLE();
 }

 /**ADC2 GPIO Configuration
 PC2 ------> ADC2_IN3
 PC3 ------> ADC2_IN4
 */
 HAL_GPIO_DeInit(GPIOC, GPIO_PIN_2|GPIO_PIN_3);

 /* USER CODE BEGIN ADC2_MspDeInit 1 */

 /* USER CODE END ADC2_MspDeInit 1 */
 }
 else if(adcHandle->Instance==ADC3)
 {
 /* USER CODE BEGIN ADC3_MspDeInit 0 */

 /* USER CODE END ADC3_MspDeInit 0 */
 /* Peripheral clock disable */
 HAL_RCC_ADC_CLK_ENABLED--;
 if(HAL_RCC_ADC_CLK_ENABLED==0){
 __HAL_RCC_ADC_CLK_DISABLE();
 }
 /* USER CODE BEGIN ADC3_MspDeInit 1 */

 /* USER CODE END ADC3_MspDeInit 1 */
 }
}

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

The minimum time period of ADC can be 2.5+12.5 clock cycles = 15 clock cycles. The timer triggers every 20 clock cycles. But, at this frequency the ADC data is missing every other sample. To get all the expected samples, I have to run the timer with period of at least 28 clock cycles. What am I missing? How can I get the ADC data for every 20 clock cycles?

Thank you. 

Best answer by Sarra.S

Hello again @kasarghu

you can refer to AN4031 on how to predict DMA latencies (section 3), with an example of ADC to SRAM DMA transfer (section 3.2.1), to get an idea on how to estimate globally as the example is applicable on F4 not L4. 

1 reply

ST Employee
July 16, 2025

Hello @kasarghu

This seems to be related to the synchronization between the timer trigger period and the ADC conversion time in dual mode with DMA; when using dual ADC fast interleave mode, the two ADCs alternately convert the same channel and the time between two successive samples is 7 ADC clock cycles.

So, if your timer triggers every 20 clock cycles, but the ADC conversion (including sampling and conversion) takes 15 cycles, the timing doesn’t line up perfectly, on top of that, DMA adds some extra delay for transferring the data.

What can happen is that the timer triggers again before the DMA has finished moving the previous conversion data. This mismatch causes the problem you described.

To fix this, you need to match the trigger period with the dual ADC interleave mode timing. The timer period must be at least the sum of these times (15 cycles + DMA latency) 

Hope that helps! 

kasarghuAuthor
Associate
July 17, 2025

That makes sense for interleave mode. But, I am using dual ADC regular simultaneous mode with full-word size MDMA (unless I made mistake in configuration somewhere).

According to the RM0351 document, 'Figure 132. DMA requests in regular simultaneous mode when MDMA = 10', both channels together should take 15 cycles + DMA latency. Could you please point me where I can get some more information on estimating DMA latency?

Thank you.

Sarra.SBest answer
ST Employee
July 22, 2025

Hello again @kasarghu

you can refer to AN4031 on how to predict DMA latencies (section 3), with an example of ADC to SRAM DMA transfer (section 3.2.1), to get an idea on how to estimate globally as the example is applicable on F4 not L4.