STM32N6 Can't program due to BOOT1 pin tied to ground
Hi, I have a custom STM32N6 board where the BOOT0 and BOOT1 pins are tied directly to ground under the BGA with no test points or jumpers. Is there anyway to connect a debugger in this scenario or is my board bricked?
Below is what I get when attempting to connect via an ST-Link V3:
>STM32_Programmer_CLI.exe -c port=SWD mode=UR -rst
-------------------------------------------------------------------
STM32CubeProgrammer v2.21.0
-------------------------------------------------------------------
ST-LINK SN : 003700163431511731343632
ST-LINK FW : V3J17M10
Board : STLINK-V3MINIE
Voltage : 3.26V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x486
Revision ID : Rev Z
Device name : STM32N6xx
Device type : MCU
Device CPU : Cortex-M55
BL Version : --
MCU Reset
Error: Unable to run MCU!
Error: Error code: 32
And this is what I get from the STM32CubeProgrammer GUI:
23:21:41:351 : UR connection mode is defined with the HWrst reset mode
23:21:41:372 : ST-LINK SN : 003700163431511731343632
23:21:41:372 : ST-LINK FW : V3J17M10
23:21:41:372 : Board : STLINK-V3MINIE
23:21:41:372 : Voltage : 3.29V
23:21:41:376 : SWD freq : 8000 KHz
23:21:41:376 : Connect mode: Normal
23:21:41:376 : Reset mode : Hardware reset
23:21:41:378 : Device ID : 0x486
23:21:41:378 : r ap 0 @0x18001004 0x00000004 bytes Data 0x00000000
23:21:41:387 : reset ap 1
23:21:41:387 : r ap 1 @0x18001004 0x00000004 bytes Data 0x00000018
23:21:41:388 : fail @0xFEEEFEEE
23:21:41:388 : Revision ID : Rev Z
23:21:41:402 : Reading data...
23:21:41:403 : r ap 1 @0x00000000 0x00000004 bytes Data 0x00000018
23:21:41:503 : r ap 1 @0x00000000 0x00000004 bytes Data 0x00000018
23:21:41:503 : Database: Config 0 is active.
23:21:41:504 : r ap 1 @0x46009024 0x00000004 bytes Data 0x00000018
23:21:41:504 : fail @0xFEEEFEEE
23:21:41:584 : r ap 1 @0x46009024 0x00000004 bytes Data 0x00000018
23:21:41:584 : fail @0xFEEEFEEE
23:21:41:592 : UPLOADING ...
23:21:41:592 : Size : 1024 Bytes
23:21:41:592 : Address : 0x34064000
23:21:41:592 : Read progress:
23:21:41:592 : Reading data...
23:21:41:592 : r ap 1 @0x34064000 0x00000400 bytes Data 0x00000018
23:21:41:683 : r ap 1 @0x34064000 0x00000400 bytes Data 0x00000011
23:21:41:683 : Error: Data read failed
23:21:41:735 : r ap 1 @0x46009024 0x00000004 bytes Data 0x00000011
23:21:41:736 : fail @0xFEEEFEEE
23:21:41:736 : r ap 1 @0x08000000 0x00000004 bytes Data 0x00000018
23:21:41:736 : fail @0xFEEEFEEE
23:21:41:736 : Warning: Connection to device 0x486 is lost
23:21:41:921 : r ap 1 @0x46009024 0x00000004 bytes Data 0x00000018
23:21:41:922 : fail @0xFEEEFEEE
23:21:41:923 : r ap 1 @0x08000000 0x00000004 bytes Data 0x00000018
23:21:41:923 : fail @0xFEEEFEEE
23:21:41:923 : Warning: Connection to device 0x486 is lost
23:21:42:131 : Disconnected
23:21:42:131 : Disconnected from device.
23:21:42:137 : Disconnected from device.
I've replicated the issue on the N6 Nucleo board and the only way to fix it there seems to be to move the BOOT1 jumper so it goes into development boot.
The flash memory is unintialised so there is no FSBL, the debug port keeps disconnecting me, I don't have access to USB/USART1/USART2/UART4, is there any other way to program an STM32N6?
Please tell me my best option isn't to insert a wires under the BGA to access USART2 then use that to change the BOOT1 pin to a more accessible pin via OTP.