Skip to main content
Visitor II
June 26, 2025
Question

STM32N6 in Nucleo XIP mode

  • June 26, 2025
  • 1 reply
  • 393 views

I have successfully completed using STM32N6 in LRUN mode and got the proper result and now I want to use Execute in place mode so please provide with all its related documents and videos.
When I try to run appli code in DEV mode it does not run, it displays "Target is not responding, retrying..." and also when i try to use xspi clock to 200MHz and main clock to 800MHz even FSBL shows the same error.

1 reply

KDJEM.1
Technical Moderator
June 27, 2025

Hello @1anku and welcome to the community;

 

Are you able to flash/run the official example Template_FSBL_XIP ?

This project is targeted to run on STM32N657X0H3QU device on NUCLEO-N657X0-Q board.

I recommend you to look to the readme file for information on how to use the Template FSBL XIP.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.