STM32N6 max power consumption versus GPIOs usage
New question from this thread.
Hi
I am using STM32N6 Nucleo-144 board. In this board VDDIO is the power supplied at VDD, VBAT. VDDIO2, VDDIO4, and VDDIO5. So this the the power supply which is driving GPIOs. This power is generated by LD39020ADTPU33R which is a LDO Voltage Regulators which can supply maximum 200 mA current.
I am worried about if i can only use 10 GPIOs? What if i need to more GPIOs in my design?