Skip to main content
matt-crc
Senior III
October 27, 2025
Solved

STM32N657 IO 3.3V tolerant?

  • October 27, 2025
  • 4 replies
  • 288 views

Hello,

I'm using the STM32N657 processor and have the HEXASPI device running at 1.8V.  

VDDIO2 is connected to 1V8 supply (which affects: PO[5..0] and PP[15..0]

The FMC is placing the A23 line on pin PO1 (this is the only option for the FMC-A23) and the FMC device is running at 3.3V.   Can I place a pullup to 3.3V on PO1, or will this affect/blow  the GPIO connected to 1.8V -OR- do I need to place a voltage translator on that pin?

 

mattcrc_0-1761602911315.png

 

Best answer by RomainR.

Hi @matt-crc 

As explained in DS14791 Rev7:

Absolute Maximum ratings (value never to be reached) Table 21. Voltage characteristics. On a TT GPIO in 1.8V HSLV mode (corresponding to programmed OTP124 HCONF and VDDIOxVRSEL = 1) the max VIN voltage = 1.98V

Table 24. General operating conditions, VIN when I/O TT_xx in the 1.8V range, max = min VDD + 0.3V.

You do not indicate the package you are using. On the VFBGA264, you have the FMC_A23 option on PB3 or PD1.

Best regards,

Romain

4 replies

AScha.3
Super User
October 28, 2025

Hi,

You cannot pull up a fast output line to another level, the internal protection diodes would prevent it. And you probably want a fast signal here, nothing slow with pullups. So take maybe a single gate as a level shifter for getting a fast output signal.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
RomainR.
RomainR.Best answer
ST Employee
October 28, 2025

Hi @matt-crc 

As explained in DS14791 Rev7:

Absolute Maximum ratings (value never to be reached) Table 21. Voltage characteristics. On a TT GPIO in 1.8V HSLV mode (corresponding to programmed OTP124 HCONF and VDDIOxVRSEL = 1) the max VIN voltage = 1.98V

Table 24. General operating conditions, VIN when I/O TT_xx in the 1.8V range, max = min VDD + 0.3V.

You do not indicate the package you are using. On the VFBGA264, you have the FMC_A23 option on PB3 or PD1.

Best regards,

Romain

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
matt-crc
matt-crcAuthor
Senior III
October 28, 2025

Hi @RomainR. 

1- yes it is the VBGA264    STM32N657X0H3Q

2- FMC-A23 is not available on A14-PD1, F13-PB3, or T17-PN2.  I attached the .ioc file if you wanted to see it.

3- I want to run the FMC at 200MHz with the address setup time = 1 cycle.  I'm not sure if a voltage converter will skew address decoding (if that is the only address line going to a voltage translator).

At this point, I'm debating if i should just remove A23 all together from the design... sigh

4- Can you confirm that on the N657, the FMC can run at 200MHz?  All I found in the reference manual was a transfer rate of 800Mbytes/sec on the FMC.

thanks, Matt

LCE
Principal II
October 28, 2025

Forget any fiddling at these speeds with pull-ups, and - what you said - even level converters might have a too high propagation delay, unless all signals are going through similar devices - which would probably take too much space.

So better change the MCU package - or as you said, check if you can remove A23. 

RomainR.
ST Employee
October 28, 2025

Hi @matt-crc 

You have assigned PB3 and PD1 for other FMC signals in your .ioc (FMC_A7 and MC_FBL1)
This is why you cannot use them for FMC_A23.
But it is available in AF14 as explained in Table 20. Alternate functions: AF8 to AF15

The FMC timing can be found in DS14791 Rev7 in 5.3.19 FMC characteristics where all timing
are based on Tfmc_ker_ck = fmc_ker_ck

If you refer to RM0486 in Table 73. Peripheral clock distribution summary (continued) indicates
max kernel clock FMC = 200MHz

You already use the biggest package. You must choose between XSPI or FMC, both seem not a possible use case.

Best regards,

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.