Skip to main content
matt-crc
Senior III
October 27, 2025
Question

STM32N657 power supply documentation not clear regarding VBAT

  • October 27, 2025
  • 3 replies
  • 196 views

Hello,

In AN5967, it says:

mattcrc_0-1761599398585.png

When VBAT is connected (VBAT = 3.0V)?  will the oscillator (RTC) stop running if VDDA18AON is not present?

There are several conflicts between the various documents... Can someone at STM update the docs?

AN5967,  RM6486, UM3300, and the STM32N657x0-dk development board schematics seem to contradict each other.... which one is correct regarding the SMPS configuration?

3 replies

Chris21
Associate II
October 27, 2025

The RTC [clock] and LSE [oscillator] are in the Backup domain for most STM32 devices:

 

Chris21_0-1761601159075.png

So VBAT or VDD is needed to keep those operating.

 

 

Technical Moderator
October 27, 2025

Hello @matt-crc 

Thank you for pointing out this topic.

 I've passed your request to our team through internal ticket number 220557 for further analysis. 

(PS: Ticket number 220557 is only for reference and follow-up to ensure that we resolve this for you).

 

 

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
matt-crc
matt-crcAuthor
Senior III
October 27, 2025

Hi @Imen.D 

Have your guys take a look at this post as well.... some other doc errors: 

SMPS on STM32N657

thanks, Matt