STM32N657L0 - uncontrolled power up and power down sequence?
Hi,
we are using the internal SMPS for core voltage generation.
VDD, VBAT and VDD18AON are on 1.8V.
My question is if I can also power up the other 1.8V lines (VDDSMPS, VDDA18USB, VDDA18CSI, VDDCSI,
VDDA18ADC and VREF+) simulteanously with VDD, VBAT and VDD18AON or does this harm the device?
So I would like to power up the 1.8V lines all together to get rid of an additional load switch on the PCB (for delaying the "late" 1.8V lines) due to space constraints. Is it possible?
Thanks a lot!