Skip to main content
clin.12
Associate
August 8, 2025
Question

STM32U083RC RTC wakeup mcu from stop mode

  • August 8, 2025
  • 1 reply
  • 648 views

I have three questions regarding the STM32U083RC:

1.Why  is the reset value of EXTI_IMR1 register 0xFFF80000?The EXTI line 19-21 is configurable lines。

2.I encountered a problem: when I used the NUCLEO-U083RC demo program to PWR_STOP2_RTC, I found that when the bit28 of the EXTI_IMR1 register was configured to 0 or 1, the RTC could wake up the MCU from stop mode. Why is the function of EXTI_IMR1 register not working?

3.Why does RTC/TAMP describe combined with EXTI lines 19 & 21 in the Vector table?

1 reply

ST Employee
September 9, 2025

Hi @clin.12

The EXTI_IMR1 register on the STM32U083RC resets to 0xFFF80000 because, by default:

  • Interrupt requests for lines 0-18 are masked (disabled)
  • Lines 19-21 are unmasked (enabled)

This setup reflects that EXTI lines 19-21 are configurable and active for interrupts out of reset, as defined in the EXTI register specifications.

 

clin.12
clin.12Author
Associate
October 13, 2025

3.Why does RTC/TAMP describe combined with EXTI lines 19 & 21 in the Vector table?