Skip to main content
Associate III
November 24, 2025
Question

STM32U5 DCMI DMA is not working as expected.

  • November 24, 2025
  • 5 replies
  • 240 views

Hello,

    We have developed an image capturing application successfully based on STM32H7xxxx and OV7725 camera. We are now targeting to port the application to target STM32U5xxxx with the same camera. But it looks the DMA doesn't works as expected. The DCMI DMA complete callback is firing with no image data in the target buffer. 

    Please guide us how to port the application from H7 to U5.

Best regards-

Shubhendu Bikash Banerjee

Attaching here snaps of the configurations we made so far.

DCMI GPIODCMI GPIO

DCMI NVICDCMI NVICDCMI parametersDCMI parametersGPDMA1 channelsGPDMA1 channelsGPDMA1 CH0GPDMA1 CH0GPDMA1 securityGPDMA1 security

Code snippet:

#define IMAGE_FRAME_WIDTH 320
#define IMAGE_FRAME_HEIGHT 240
#define IMAGE_BYTES_PER_PIXEL 2
#define IMAGE_BYTES_COUNT (IMAGE_FRAME_HEIGHT * IMAGE_FRAME_WIDTH * IMAGE_BYTES_PER_PIXEL)
static uint32_t gDCMIBuff[IMAGE_BYTES_COUNT / sizeof(uint32_t)] = { 0 };
static volatile bool gWaitForFrame = false;

CaptureFrame{
	gWaitForFrame = true;
	halReturn = HAL_DCMI_Start_DMA(&hdcmi, (uint32_t) DCMI_MODE_SNAPSHOT,
			(uint32_t) gDCMIBuff, (uint32_t) imageSize);
	if (HAL_OK != halReturn) {
		SERVICE_LOGE(TAG, "DCMI start error: 0x%.8X", HAL_DCMI_GetError(&hdcmi));
		exeStatus = ERROR_GEN_FAILURE;
		goto label_exitPoint;
	}

#if LOG_LEVEL >=LOG_LEVEL_DEBUG
	SERVICE_LOGD(TAG, "Frame capture started.");
#endif

	while (gWaitForFrame) {
		__asm__("nop");
	}
	HAL_DCMI_Stop(&hdcmi);
	SetCameraToSleep(pvCameraSensor);
}

void HAL_DCMI_FrameEventCallback(DCMI_HandleTypeDef *hdcmi) {
	HAL_DCMI_Stop(hdcmi);
	gWaitForFrame = false;
}

 

@mƎALLEm 

@Federica Bossi 

 

This is for reference:

@devjeetmandal09 

5 replies

ScottyWinsome
Associate II
November 26, 2025

This sounds very similar to my observation wrt the STM32U5 GPDMA for SPI, specifically what I saw using DMA for SPI3 RX and TX: both the TX and RX GPDMA 'TC' IRQ's fired (in that order TX then RX) and I saw the SPI3 SCLK clocking, but no data on the SPI3 MOSI (and thus no data in buffer pointed to by DMA for SPI MISO, since I jumper-wire loopback the MOSI data).
https://community.st.com/t5/stm32-mcus-products/stm32u5-spi-gpdma-cannot-get-simple-loop-back-data-working/td-p/858555


I will bookmark your post to see if you find a solution first.

Associate III
November 28, 2025

Update:

    I can now capture frames. But there is a problem, the frame get's splitted in the buffer. The scenario looks like a horizontal part from lower part of the frame is placed at upper position.

SampleSample

KDJEM.1
Technical Moderator
December 11, 2025

Hello @shubhenduatadben ,

 

What is the DCMI_PIXCLK frequency? Could you please try reducing the clock frequency.

I recommend you to look at DCMI_ContinousCap_EmbeddedSynchMode example and precisely the DCMI_ContinousCap_EmbeddedSynchMode.ioc file and get inspired to check the DCMI and GPDMA configuration.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
December 12, 2025

Hi @KDJEM.1 

Thank you for your suggestions. I can't reduce the DCMI_PIXCLK, which is running at 12MHz right now. As I can remember, current DCMI_PIXCLK is well under DCMI spec. 

I've found that the DCMI is filling the buffer assuming the frame as square,i.e. the current WIDTH x HEIGHT = 320 x 240 but the DCMI assumes frame of 320 x320.

If I provide a 320 x 320 compatible buffer, the DCMI is collecting the frame but the top 80 lines are blank(black) and I get the actual image as 320 x 240.

 

KDJEM.1
Technical Moderator
December 12, 2025

Hello @shubhenduatadben ,

 

Thank you for updating post and for these information.

For this resolution, I recommend you to enable the GPDMA circular mode.

Please  let me know if the issue is solved or not?

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
December 24, 2025

GPDMA is in circular mode. Yet producing the result.

Visitor II
January 9, 2026

We are experiencing a similar issue using HAL_DCMI_Start_DMA. Have configured a two node linked list in circular mode (SetCircularModeConfig) for DMA with an OV5640 in JPEG mode at full resolution. Here is an example image frame captured. Notice the horizontal issue at the top as well as along the right edge.


capture_20260108_212245_008_jpeg.jpg
Investigation shows that the DMA is filling the target PSRAM memory buffer with a large gap at the start (explains the top black horizontal line). We ended up switching to manually controlling the ping-pong buffer using the XferCpltCallback directly on the DMA_HandleDefType object and managing the buffers ourselves. All worked fine after that. Is there possibly a bug in how HAL_DCMI_Start_DMA handles the ping-pong buffers?