Skip to main content
Associate II
June 23, 2025
Question

STM32U5 Serial Bootloader AN3155 Discrepancy

  • June 23, 2025
  • 1 reply
  • 330 views

In looking at AN3155, USART protocol used in the STM32 bootloader, the following diagram describes the MCU's write protect command sequence from the device side:

dsurrett_1-1750720697920.png

There is a comment at the bottom which indicates that only certain F and L series chips perform the system reset.  I am working with a STM32U585QI, and I also see that this chip appears to perform a system reset when executing the write protect command.  Is that correct and this comment is just wrong, or am I seeing this unexpectedly?

1 reply

Technical Moderator
June 24, 2025

Hello @dsurrett ,

The note in the AN3155 is correct. A system reset when executing the write protect command doesn’t apply to STM32U5.

On the STM32F4/F7/L4 series listed on the AN3155, modifying the Option byte doesn’t generate a reset – it’s bootloader SW who add a NVIC_SystemReset after any OB change. But for the new STM32 we removed that as it’s not aligned with the HW behaviour.

Now, if a product generates a system reset after modifying the OB, this is due to the HW itself:

  • For example: STM32U5/L5/WBA.. generate a reset when OB_LAUNCH is done, so when OB is modified
  • This is not true on product like STM32H7, STM32H5..

You can refer to the RM0456 related to your product and check this detailed on "Embedded flash memory (FLASH)" part.

Hope I answered to your question and this clear for you now.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"