Skip to main content
Visitor II
January 6, 2026
Question

The 48MHz crystal oscillator for HSE of STM32H743 cannot be realized.

  • January 6, 2026
  • 3 replies
  • 347 views

Hello sir/miss , 

According to the STM32H7 datasheet, the range of the HSE external crystal oscillator is 4M - 48MHz. However, when we used the STM32H7IIT6-EVAL evaluation board and replaced the original 25MHz surface mount passive crystal oscillator with a 48MHz passive crystal oscillator, we were unable to obtain the corresponding 48MHz frequency from the MCO-PA8 pin.

Summary: All conventional passive crystals from 4M to 40MHz were tried and worked fine. However, for external passive crystals above 40MHz , just like 48MHz, the MCO output waveform frequency was 16MHz, which is 1/3 of the HSE frequency, and it was unable to output 48MHz.

Please provide a solution or suggest areas where we can improve the test. Thank you very much!

3 replies

RobK1
Associate II
January 6, 2026

You chose a crystal that works in 3rd overtone mode.

 

Be sure to select one that works in fundamental mode:

Crystals | Electronic Components Distributor DigiKey

mƎALLEm
Technical Moderator
January 6, 2026

Hello,


@shaunSHAUN wrote:


Summary: All conventional passive crystals from 4M to 40MHz were tried and worked fine. However, for external passive crystals above 40MHz , just like 48MHz, the MCO output waveform frequency was 16MHz, which is 1/3 of the HSE frequency, and it was unable to output 48MHz.


From this statement I suspect a failing HSE oscillation startup.

So when you replaced that crystal, did you check if that crystal is compatible with STM32?

Please read this article: How to select a compatible crystal and load capacitors for STM32 with layout guidelines

+ Refer to the application note AN2867 "Guidelines for oscillator design on STM8AF/AL/S and STM32 MCUs/MPUs"

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
AScha.3
Super User
January 6, 2026

HI,

so for the "48MHz" crystal you picked a third overtone type, that will its fundamental resonate at 16M.

1. try with a crystal thats in fundamental mode or a crystal oscillator (+ HSE bypass setting)

2. why try/using crystal at the given limits ? Never a good idea... Better to stay in middle of possible range.

"If you feel a post has answered your question, please click ""Accept as Solution""."