Skip to main content
zyimi
Associate
July 28, 2025
Question

The F429 uses both SDRAM and SRAM

  • July 28, 2025
  • 1 reply
  • 155 views

Whether the two buses can be used at the same time? Winbond's SDRAM is used to find a high probability of reading and writing errors in SDRAM data。 but there is no problem with using ISSI. If you don't read or write to the external SRAM, it's fine。

1 reply

TDK
Super User
July 28, 2025

Yes, SRAM and SDRAM can be used at the same time. Try slowing the SDRAM clock rate down by a factor of 10, could be a layout or noise issue.

"If you feel a post has answered your question, please click ""Accept as Solution""."