Typo in STM32L412xxx Datasheet?
I'm looking at Rev 9 of the STM32L412xxx Datasheet, as linked on Digikey, and I'm having a hard time understanding the current consumption figures specified for the Low-power Run & Low-power Sleep modes on the MCU. Per the table on pg.24 (shown below), the current draw is 83uA/MHz in LPRun mode, which is higher even than the normal Run mode up to 26MHz (range2), which doesn't make sense to me. Further, the current draw in LPSleep mode is also 83uA/MHz, which suggests there's no power savings putting the MCU to sleep in Low-power mode? Can somebody tell me what I'm missing here, or is this a typo and one or both of those figures are wrong?