UCPD G0 Disco board in SPY mode doesn't show up as a USB device (STM32G071B-DISCO)
So i have the stm32G0 usb-c disco board.
https://www.st.com/en/evaluation-tools/stm32g071b-disco.html
I've flashed the latest USBPD_Analyzer software on the device and i have the latest UCPD monitor project.
The semi problem is that it's kind of frustrating that in SPY MODE by default the mico doesn't show as a USB device. I only see the usb micro usb connection when i'm in Snk Mode. Is there a reason why in spy mode the USB connection to the PC from the micro doesn't show up?
So what i have to do is. Start in Snk mode. Connect to the PC via the micro usb connector and connect to the UCPD monitoring program. Then i can switch to SPY MODE then i can attach my devices to it. Which can kind of be flakey some times.