Question
USB_DEVICE Not Recognized on STM32L562CEU6P Board
- June 19, 2025
- 1 reply
- 573 views
Hi everyone,
I'm developing on an STM32L562CEU6P board using STM32CubeIDE on a Windows 11 laptop.
In my project, I'm trying to use the USB_DEVICE feature, but when I run the project, my computer fails to recognize the USB device.
What I've tested so far:
- I tested the same board on a desktop computer running Windows 10 – the USB device was recognized successfully.
- I tested a different board (NUCLEO-F767ZI) on my laptop – it was recognized without issues.
- I verified that the physical connection is fine, drivers are installed, and there are no hardware issues.
My questions:
- Could there be a difference in USB recognition between desktop and laptop computers?
- Could this issue be related to the operating system (Windows 11 vs. Windows 10)?
- Are there any specific drivers or settings required for the STM32L562CEU6P board?
I’d really appreciate any help, suggestions, or insights :folded_hands:
Thanks!