Skip to main content
Associate
December 14, 2024
Solved

USB UVC with STM32U5G9ZJT6Q is 60 MHZ PHY Clock possible

  • December 14, 2024
  • 1 reply
  • 531 views

Hello everyone,

I am currently working on a project using the STM32U5G9ZJT6Q mcu with USB UVC. For my setup, I am providing: 

32 MHZ external clock to phy 

144 MHZ system clock 

In the documentation(TRM and CubeMX), the maximum external phy clock specified is 32 MHZ.

However I need to achieve a 60 MHZ PHY Clock, which seems to be supported by the hardware but isn't explicitly listed in CubeMX or the reference manual.

My questions are: 

Is it possible to configure the external PHY Clock to run at 60 MHZ? 

If so, does anyone have an example configuration or code snippet to achieve this?

Any insights or suggestions would be greatly appreciated!

Thank you in advance.

Best answer by FBL

Hi @AA22 

Would you attach your IOC file? Based on the datasheet, STM32U5G embeds HS PHY internally. Why would you configure it with 60MHz?

FBL_0-1769435214409.png

 

1 reply

FBLBest answer
Technical Moderator
January 26, 2026

Hi @AA22 

Would you attach your IOC file? Based on the datasheet, STM32U5G embeds HS PHY internally. Why would you configure it with 60MHz?

FBL_0-1769435214409.png

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL