Skip to main content
Associate II
June 26, 2025
Solved

VBAT on STM32U5G9J-DK1

  • June 26, 2025
  • 1 reply
  • 605 views

Hello,

I have got an STM32U5G9J-DK1 and I want to use its VBAT pin which has been connected to the signal VDD_MCU, which is internal to the board, via solder bridge SB29. As far as my understanding of the data sheet goes, the VBAT pin is supposed to be fed with 1.8 V. So, I was thinking to remove the solder bridge and connect an appropriate battery for this operation. Could you suggest me some good batteries that would suffice this requirement?

Thanks in advance.

Regards,

Gaurav.

Best answer by MHoll.2

VBAT is a separeted power domain, that can be powered up to 3.6V indipendend of the other power domains. So yes You can have a CR2035 (3V) on the VBAT pin and 1.8V on VDD / VDD_CPU.

1 reply

MHoll.2
Senior III
June 26, 2025

The Voltage range on VBAT is 3.6V down to 1.65V, The required battery depend's on the current consumed and the time the battery has to last. Normaly I'm using CR2032 or similar battery's.

Associate II
June 26, 2025

The datasheet repeatedly mentions, "The STM32U5x9J-DKx Discovery kits are low-power systems designed for VDD and VDD_MCU at 1.8 V only." Also, at the top of the block diagram on page #8, it clearly says, "1.8 V power supply." So wouldn't there be an issue if I feed VBAT something other than 1.8 V?

MHoll.2
MHoll.2Best answer
Senior III
June 26, 2025

VBAT is a separeted power domain, that can be powered up to 3.6V indipendend of the other power domains. So yes You can have a CR2035 (3V) on the VBAT pin and 1.8V on VDD / VDD_CPU.