Skip to main content
Associate II
March 26, 2026
Solved

VDD33USB connection problem when not using USB

  • March 26, 2026
  • 2 replies
  • 136 views

Hi,

I do not plan to use USB, and the STM32N6's VDD is 1.8V.

However, creating a new 3.3V power supply just only for the VDD33USB pin is too inefficient.

The datasheet lists the absolute maximum ratings for VDD33USB as ranging from 0V to 3.6V when USB is not used, and the comment below states the following:

1. All main power and ground pins must always be connected to the external power supply, in the permitted range.

Therefore, Finally if I do not plan to use USB on the STM32N6, which of the following options should I choose for the VDD33USB pin?
(have to consider leakage current in stop mode)

1) NC
2) 3.3V (by creating a new power supply)
3) 1.8V
4) GND

thanks in advance.

Best answer by FBL

Hi @AndersonKKK 

With all external interfaces at 1.8 V, since you are not using USB, you can safely tie VDD33USB to GND to minimize leakage and avoid generating 3.3 V.

2 replies

TDK
Super User
March 26, 2026

If you're not using USB, you can ground VDD33USB.

Screenshot 2026-03-25 211703.png

You may want to tie it to VDD instead if you need margin on the UCPD pins. But if everything coming in is 1.8 V, no issues with grounding it.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
FBLBest answer
Technical Moderator
March 26, 2026

Hi @AndersonKKK 

With all external interfaces at 1.8 V, since you are not using USB, you can safely tie VDD33USB to GND to minimize leakage and avoid generating 3.3 V.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL