VDDCSI, VDD33USB pin on STM32N6
Hi,
I do not plan to use USB or CSI, and the board only receives 1.8V power. So, I asked how to connect the VDD33USB pin, and I was told to just connect it to GND. However, I have two more questions.
I currently have the VDDA18USB and VDDA18CSI pins connected to 1.8V. Is it okay to leave them as they are, or would it be better to connect them to GND? (have to consider leakage in the Stop mode)
Also, should I connect VDDCSI to GND as well?
Thanks in advance.