Accessing "Backup SRAM" with RDB Level 1 from Code in RAM
Hi all,
I am not sure if I understood the reference manual right: When I activate Read Out Protection RDP Level 1, I can no longer access RTC Backup registers if I execute in RAM. I did not read that also Backup RAM is inaccessible. But it looks it is the case...
My problem is that I use the 128k version of the STM32H7 and I must run the firmware in RAM. But I also need a low power retenion memory. Leaving D3 on to keep SRAM4, uses too much power (few mA). HAL_PWR_EnterSTANDBYMode() from hal_pwr.c works fine for me - except that it clears SRAM4.I tried other STOP modes but the source too much. BTW there is no tamper alarm activated (at least not by me).
Is there a way accessing Backup SRAM from code running in AXI/SRAM1,2,3 etc?