Skip to main content
Olivier FAURAX
Associate II
November 24, 2017
Solved

Adding option byte RDP level 1 prevents project from starting

  • November 24, 2017
  • 1 reply
  • 2865 views
Posted on November 24, 2017 at 15:08

I have a simple project that toogle a LED. I try to add software protection to it.

Basically, it does  :

main()

{

  Init_GPIO_for_LED();

  LED_ON();

  while(i++ < 10000000) {}; // yes, ugly

  LED_OFF();

 

  while(1) {} // wait forever

}

If I flash it, I see the LED light for some time.

Then, I want to protect the program, so I use the ST-Link Utility to switch the RDP to Level 1.

$ ST-LINK_CLI.exe -OB RDP=1

STM32 ST-LINK CLI v3.0.0.0

STM32 ST-LINK Command Line Interface

ST-LINK SN : [edited]

ST-LINK Firmware version : V2J24M11

Connected via SWD.

SWD Frequency = 4000K.

Target voltage = 0.0 V.

Connection mode : Normal.

Device ID:0x429

Device flash Size : 64 Kbytes

Device family :STM32L100x6xxA/L15xx6xxA

Updating option bytes...

Option bytes updated successfully.

I perform a hard reset after, and I can see the RDP level is set :

$ ST-LINK_CLI.exe -rOB

STM32 ST-LINK CLI v3.0.0.0

STM32 ST-LINK Command Line Interface

ST-LINK SN : [edited]

ST-LINK Firmware version : V2J24M11

Connected via SWD.

SWD Frequency = 4000K.

Target voltage = 0.0 V.

Connection mode : Normal.

Device ID:0x429

Device flash Size : 4095 Kbytes

Device family :STM32L1xxx4xxA-xxx6xxA-xxx8xxA

Option bytes:

RDP         : Level 1

BOR         : Level 0

IWDG_SW     : 1

nRST_STOP   : 1

nRST_STDBY  : 1

Data0       : 0x00

Data1       : 0x00

SPRMOD      : 0

WRP         : 0x00000000

But now, there is no LED light at all. It seems the program doesn't start.

I can switch back to level 0, and the flash is mass erased, as explained in the docs, but I need level 1 to read-protect the code.

I'm on a STM32L151C8T6A, and the LED pin is the M19.

What's wrong?

Thanks in advance.

#rdp #protection #flash
This topic has been closed for replies.
Best answer by Olivier FAURAX
Posted on December 01, 2017 at 13:15

The problem was in the hardware

There was a capacitor that prevented the complete reset of the  STM32, so there was no restart from the beginning of the program!

1 reply

Olivier FAURAX
Olivier FAURAXAuthorBest answer
Associate II
December 1, 2017
Posted on December 01, 2017 at 13:15

The problem was in the hardware

There was a capacitor that prevented the complete reset of the  STM32, so there was no restart from the beginning of the program!