Skip to main content
Alex Hösl
Associate
September 9, 2019
Question

Can't reset RDP from level 1 to level 0; Nucleo L476RG

  • September 9, 2019
  • 1 reply
  • 799 views

Hi,

I was testing with the Nucleo STM32L476RG board, BSP example project FLASH_DualBoot.

I made small changes in the example code (LED blink stuff) and programmed bank 1 and 2 several times. I also manually checked/toggled the option bytes BFB2 bit a few times.

When I tried to program the MCU flash bank 2 again with STM32 ST-LINK Utility it said that it's not possible because of read/write protection. I didn't configure it any time before, only using the BFB2 bit in the example code. In the option bytes window I discovered that "Read/Write Protection Bank B" was activated. I couldn't uncheck it, because it says:

"To disable Read/Write protection of BANK B, you must set PCROP_RDP bit, and switch RDP from Level 1 to Level 0".

Well, both we're in desired state. Power cycle doesn't help. So I tried to trick the MCU by switching from Level 0 to Level 1 to be able to revert from 1 to 0.

But it doesn't let me revert from 1 to 0:

"ERROR: Could not set Option bytes! Please reset the target and retry."

"Warning: Can not read memory! Disable Read Out Protection and retry."

I retried several times, tried to load some code, tried to update the onboard ST-Link of the Nucleo board, power cycle...what's the matter with this problem? Is the MCU lost in a broken state? Any suggestions?

STM32 ST-LINK Utility V4.4.0; STM32Cube_FW_L4_V1.14.0

Regards,

Alex

This topic has been closed for replies.

1 reply

Alex Hösl
Associate
September 9, 2019

... by the way: I wasn't able to post in Communities forum:

"Review the errors on this page.

  • You can't add new topics, so select existing topics for your post"