Core Locked Up (STM32h753ZI)
Hi,
I am Working on SBSFU. I have Flashed the STM32H753zi example code after flashing i am not able to flash from programmer. even after changing the option bytes RDP level 0 is set.
I have Connect another working board of stm32h753zi board i compared the parameter with flash able baord and non-flash able board.
only one thing is observed
1.not flash able board PCROP is set to :(prot_area_start1 0x00)
2.flash able baord PCROP is set to :(prot_area_start1 0xFF)
I have tried using STMCubeProgarmmer not able modify prot_area_start1 0x00 to prot_area_start1 0xff Facing error i have attached the Screenshot below GUI and CLI both
3.Image 1 stm32Cubeprogrammer GUI:

4.Image 2stm32cubeprogrammer CLI:

Regards,
Prakash R