CPU is locked while disabling the TrustZone on the STM32U575ZIQ Nucleo board. I set level to DC(level1) and now I am not able to connect the board to Cube Programmer and throws "Connection to target must be established before performing the read comm
I was using this above video for reference. I had TrustZone enabled on the board and wanted to disable it. As per the video I first set it to DC from AA level in cube programmer. Then disconnected the board and power cycle. Then tried to connect back for the next steps, the cube programmer started throwing an error " Error: Connection to target must be established before performing the read command." Now I am not able to flash the code in Keil and it says "CPU is locked up"