Determine the padding to save the firmware SHA256 using STM32F746GDISCOVERY to verify integrity
I am trying to implement a firmware integrity check using the Cryptographic Library (X-CUBE-CRYPTOLIB) for this I have to calculate the SHA256 checksum and then determine the padding and include it in the binary that I will upload to the board.
I've been watching STM's mooc Security part 4
https://www.youtube.com/watch?v=RahlfYJ1gDs&list=PLnMKNibPkDnF0wt-ZI74SflnsBV4yKzkO&index=7
And in the lab they do the verification for a stm32g0. The problem is that I do not know how to determine the size of the firmware, in the laboratory they use the page size but on my board the flash memory has blocks of different sizes:
I also have an external memory to which I also want to make the SHA256 calculation. This memory consists of 256 blocks of 64k (These are all the same size).

Another difficulty I have is that the hex file covers two sectors (internal and external flash) so I don't know whether to put the internal and external hashes separately (just after the FW zone hit).