Skip to main content
EEdwa.1
Associate III
August 28, 2020
Solved

Download firmware by YMODEM failed at Linux

  • August 28, 2020
  • 1 reply
  • 1323 views

I build Projects "NUCLEO-G071RB" in X-CUBE-SBSFU and load "SBSFU.bin" into the board.

After reset the board, I download firmware "UserApp.sfb" with SecureCRT by using menu "Transfer > Send Ymodem" , but it failed.

I also try to use "Tera Term", it download firmware successfully. But the "Tera Term" only have Windows version.

I need download firmware from Linux, Does anybody know which tool can download firmware by YMODEM successfully at linux?

This topic has been closed for replies.
Best answer by Jocelyn RICARD

Hello,

the next release of SBSFU 2.4.0 will support minicom

This release should be available on st.com next week

Best regards

Jocelyn

1 reply

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
August 28, 2020

Hello,

the next release of SBSFU 2.4.0 will support minicom

This release should be available on st.com next week

Best regards

Jocelyn

EEdwa.1
EEdwa.1Author
Associate III
September 2, 2020

Thanks for the update. I will wait for the SBSFU 2.4.0 and try again.