Skip to main content
BEnge.1
Associate III
May 20, 2022
Question

How can I store a private ECDSA key in the KMS as a dynamic object ?

  • May 20, 2022
  • 5 replies
  • 1922 views

I would like to store two keys in the KMS as dynamic objects to use them in my UserApp project:

  • One public ECDSA key
  • One private ECDSA key

For the public key, I have as example the SBSFU_ECDSA_1_Verify key so this should be fine. However, I don't know how to add a ECDSA private key. Is that explained somewhere? I find very little information about the KMS.

Thanks in advance,

Benjamin

This topic has been closed for replies.

5 replies

Jocelyn RICARD
ST Employee
May 20, 2022

Hello @BEnge.1​ ,

documentation about this feature can be found in

1) UM2262

2) AN5056

The principle is to generate an authenticated, encrypted blob using the 2_Images_KMS_Blob project.

Once blob is created you download it using same principle as a firmware update.

After reset, SBSFU installs the new key in the KMS.

Best regards

Jocelyn

Fred
ST Employee
May 21, 2022

Agree with Jocelyn, just pay attention to the parameters to declare the object in the BLOB project: ECDSA private key objects (object class CKO_PRIVATE_KEY, key type CKK_ECDSA) hold ECDSA private keys.

Fred
ST Employee
May 23, 2022

I checked with my KMS colleague and unfortunately KMS does not provide the ECDSA sign service.

So, yes, you can declare the key and store it but KMS will not be able to use it.

The declaration must follow these rules:

PKCS #11 Cryptographic Token Interface Current Mechanisms Specification Version 2.40 (oasis-open.org)

see section 2.3.4

BEnge.1
BEnge.1Author
Associate III
May 23, 2022

@Fred​ Thank you for the precision. So If i am not able to use it, I think I will go for another algorithm (RSA) as I can see from the provided example project that it is possible to sign and verify using RSA.

If I use openssl to generate a RSA key pair, do you know how I can translate the .pem files to these objects :

(public)

0693W00000NqTDPQA3.png 

(private)

0693W00000NqTDeQAN.pngThanks,

Benjamin

Fred
ST Employee
May 23, 2022

There is an example of encoding in "kms_blob_example_keys.c".

But I can check with the colleague who developed it how he created the data.

BEnge.1
BEnge.1Author
Associate III
May 23, 2022

Yes I saw the example but I was wondering how the data was generated. I think the required information can be found using

openssl rsa -in <my_key.key> -noout -text

but if you can check with your colleague that would be very much appreciated.

Fred
ST Employee
May 25, 2022

Unfortunately, nobody had to store lots of keys, so the colleagues who worked on it made the mapping manually.