How to change read out protection from level 1 to level 0 with STM32CubeProgrammer?
Background information : we are using STM32F407 for our product and 2 of them (out of 3) encounters the same problem: RDP level has been changed from level 0 to level 1 and stopped working without any modification from our part. Before even thinking of solving the problem, we would like to switch back from RDP level 1 to level 0.
This problem is exactly the same than the one discussed here 7 years ago and where no solutions are given.
One way to do so is by using STM32CubeProgrammer. Here is what I tried:
- Open STM32CubeProgrammer
- Connect to the µC via ST-LINK: the data read failed because of RDP level
14:29:10 : STM32CubeProgrammer API v2.8.0
14:29:24 : Warning: Device changed, refreshing...
14:29:24 : ST-LINK SN : 50FF70067867515335590967
14:29:24 : ST-LINK FW : V2J29S7
14:29:24 : Board : --
14:29:24 : Voltage : 3.18V
14:29:24 : SWD freq : 4000 KHz
14:29:24 : Connect mode: Normal
14:29:24 : Reset mode : Software reset
14:29:24 : Device ID : 0x413
14:29:24 : Revision ID : Rev 2.0
14:29:24 : UPLOADING OPTION BYTES DATA ...
14:29:24 : Bank : 0x00
14:29:24 : Address : 0x40023c14
14:29:24 : Size : 4 Bytes
14:29:24 : UPLOADING ...
14:29:24 : Size : 1024 Bytes
14:29:24 : Address : 0x8000000
14:29:24 : Read progress:
14:29:24 : Error: Data read failed- Open the "Option bytes" tab
- Notice that the RDP value is 0xFF (level 1 as per the documentation)
- Change the value to 0xAA (for level 0) and click on "Apply" (with max verbosity)
14:33:54:632 : Option byte command : -ob RDP=170
14:33:54:639 : PROGRAMMING OPTION BYTES AREA ...
14:33:54:640 : Bank : 0x00
14:33:54:640 : Address : 0x40023c14
14:33:54:640 : Size : 4 Bytes
14:33:54:641 : OB buffer: edaaff0f
14:33:54:642 : Buffer program...
14:33:54:654 : halt ap 0
14:33:54:656 : w ap 0 reg 15 PC (0x20000000)
14:33:54:656 : w ap 0 reg 17 MSP (0x20000500)
14:33:54:656 : w ap 0 reg 16 xPSR (0x01000000)
14:33:54:669 : w ap 0 @0x20000C20 0x00000200 bytes Data 0x00000000
14:33:54:670 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
14:33:54:674 : w ap 0 @0x20000004 0x000007F4 bytes Data 0xF000B580
14:33:54:674 : w ap 0 @0x20000C20 0x00000004 bytes Data 0x0FFFAAED
14:33:54:675 : Loader write option bytes...
14:33:54:675 : Init flashloader...
14:33:54:675 : halt ap 0
14:33:54:675 : w ap 0 reg 0 R0 0x00000001
14:33:54:675 : w ap 0 reg 1 R1 0x00000000
14:33:54:675 : w ap 0 reg 2 R2 0x00000000
14:33:54:675 : w ap 0 reg 3 R3 0x00000000
14:33:54:675 : w ap 0 reg 4 R4 0x00000000
14:33:54:675 : w ap 0 reg 5 R5 0x00000000
14:33:54:675 : w ap 0 reg 6 R6 0x00000000
14:33:54:675 : w ap 0 reg 7 R7 0x00000000
14:33:54:675 : w ap 0 reg 8 R8 0x00000000
14:33:54:676 : w ap 0 reg 9 R9 0x00000000
14:33:54:676 : w ap 0 reg 10 R10 0x00000000
14:33:54:677 : w ap 0 reg 11 R11 0x00000000
14:33:54:677 : w ap 0 reg 12 R12 0x00000000
14:33:54:677 : w ap 0 reg 13 SP 0x00000000
14:33:54:677 : w ap 0 reg 14 LR 0x20000001
14:33:54:681 : w ap 0 reg 15 PC 0x20000005
14:33:54:681 : w ap 0 reg 16 xPSR 0x01000000
14:33:54:681 : w ap 0 reg 17 MSP 0x20000BF4
14:33:54:682 : w ap 0 reg 18 PSP 0x00000000
14:33:54:682 : run ap 0
14:33:54:682 : halt ap 0
14:33:54:683 : r ap 0 reg 0 R0 0x00000001
14:33:54:687 : w ap 0 reg 0 R0 0x40023C14
14:33:54:688 : w ap 0 reg 1 R1 0x00000004
14:33:54:690 : w ap 0 reg 2 R2 0x20000C20
14:33:54:690 : w ap 0 reg 3 R3 0x00000002
14:33:54:690 : w ap 0 reg 4 R4 0x00000000
14:33:54:692 : w ap 0 reg 5 R5 0x00000000
14:33:54:692 : w ap 0 reg 6 R6 0x00000000
14:33:54:693 : w ap 0 reg 7 R7 0x00000000
14:33:54:693 : w ap 0 reg 8 R8 0x00000000
14:33:54:694 : w ap 0 reg 9 R9 0x00000000
14:33:54:694 : w ap 0 reg 10 R10 0x00000000
14:33:54:694 : w ap 0 reg 11 R11 0x00000000
14:33:54:694 : w ap 0 reg 12 R12 0x00000000
14:33:54:694 : w ap 0 reg 13 SP 0x00000000
14:33:54:694 : w ap 0 reg 14 LR 0x20000001
14:33:54:694 : w ap 0 reg 15 PC 0x200000AB
14:33:54:694 : w ap 0 reg 16 xPSR 0x01000000
14:33:54:694 : w ap 0 reg 17 MSP 0x20000BF4
14:33:54:694 : w ap 0 reg 18 PSP 0x00000000
14:33:54:694 : run ap 0
14:33:57:969 : UPLOADING OPTION BYTES DATA ...
14:33:57:969 : Bank : 0x00
14:33:57:969 : Address : 0x40023c14
14:33:57:969 : Size : 4 Bytes
14:33:57:970 : Reading data...
14:33:57:971 : r ap 0 @0x40023C14 0x00000004 bytes Data 0x0FFFFFED
14:33:57:972 : OPTION BYTE PROGRAMMING VERIFICATION:
14:33:57:972 : Error: Expected value for Option Byte "RDP": 0xAA, found: 0xFF
14:33:57:980 : Error: Option Byte Programming failed
14:33:58:009 : UPLOADING OPTION BYTES DATA ...
14:33:58:009 : Bank : 0x00
14:33:58:009 : Address : 0x40023c14
14:33:58:010 : Size : 4 Bytes
14:33:58:010 : Reading data...
14:33:58:010 : r ap 0 @0x40023C14 0x00000004 bytes Data 0x0FFFFFEDWhat do I do wrong? Why can't I changed the RDP level back to 0?