How to reset STM32L4 after activating ReadOut Protection Level 1?
Hello!
I have a problem with STM32L496RG booting from flash after activating readout protection level 1. The issue is that MCU seems to get stuck in system bootloader code. The only way to get it to boot from main flash is to apply power on reset.
Accroding to RM0351 section 3.5.1 the readout protection is activated by system reset or power-on reset if debug was active. In my case I have no debugger connected and still the system reset is not enough to activate RDP and boot from main flash.
I have tried activating readout protection option bit via STM32CubeProgrammer and also from my firmware. In firmware, after calling HAL_FLASH_OB_Launch() the MCU ends up in unknown state where it does not respond to system bootloader command nor start executing program from main flash.
In my application I have backup power source constantly connected and there is no easy way for end user to apply power-on reset after firmware update. Is it known bug/feature for this device or am I doing something wrong? Is there any possible way to reset the MCU after RDP is activated?