How to revert from TZEN to non secure mode
Hi
I am using STM32L562 and sampled and flashed the Zephyr OS example for TrustMode.
I could not revert back the TrustZone therefore followed the information from the link https://community.st.com/t5/stm32-mcus-security/reverting-option-byte-configuration-after-tf-m-testing-in/m-p/584225/highlight/true#M5879
However, after executing the first two commands the board doesn't respond to the command. Even with the hotplug mode, I can't set RDP level back to 0
STM32_Programmer_CLI -c port=SWD mode=hotplug reset=SWrst -ob RDP=0xAA UNLOCK_1A=1 UNLOCK_1B=1 UNLOCK_2A=1 UNLOCK_2B=1
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
ST-LINK SN : 0046003F3137510C33333639
ST-LINK FW : V3J16M8
Board : STM32L562E-DK
Voltage : 3.27V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x472
Revision ID : Rev Z
Device name : STM32L5xx
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0x0
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022040
Size : 32 Bytes
Error: Uploading Option Bytes bank: 0 failed
Error: Initializing the Option Bytes failed
STM32_Programmer_CLI -c port=SWD mode=hotplug reset=SWrst -ob RDP=0xAA UNLOCK_1A=1 UNLOCK_1B=1 UNLOCK_2A=1 UNLOCK_2B=1
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
ST-LINK SN : 0046003F3137510C33333639
ST-LINK FW : V3J16M8
Board : STM32L562E-DK
Voltage : 3.27V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x472
Revision ID : Rev Z
Device name : STM32L5xx
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0x0
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022040
Size : 32 Bytes
Error: Uploading Option Bytes bank: 0 failed
Error: Initializing the Option Bytes failed
I can connect to the device
STM32_Programmer_CLI -c port=SWD mode=hotplug reset=SWrst
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
ST-LINK SN : 0046003F3137510C33333639
ST-LINK FW : V3J16M8
Board : STM32L562E-DK
Voltage : 3.27V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x472
Revision ID : Rev Z
Device name : STM32L5xx
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0x0Would you kindly help me to revert back?