How to use BOOT0 in SBSFU?
Hi all,
I am porting the SBSFU to the custom STM board which is running in the Stm32L476JGYx.
Normally user button is connected to the PC13 in the Nucleo board and in my custom PCB I made the user button for the Boot0 (PD7) I use this only for the bootable purpose,
I am having a problem changing the BOOT0 pin, I changed the default pin PC13 to PD7 using the Stm32l4xx_nucleo.h in the BSP folder but I am not getting the bootable update window (to update using the Ymodem protocol) if I do the same as in the Nucleo board. Are there any other facts should I consider when changing the User Button.
Thanks
Roshan