How to validate firmware in custom user application for STML4+ SBSFU?
For sbsfu in the following parts:
In AN5056 rev6, see section 8.5 How to validate a firmware image.
In UM2262 rev8, Appendix J
It says: At the first user application start-up, if the execution is correct (for example after self-tests execution) the user application must call a running service SE_APP_Validate(slot_id) if available or update dedicated flags in RAM otherwise to validate the firmware image.
What dedicated flags are those? How can I know about the slot_id?