I have ported X-CUBE-SBSFU to my own board successfully and can update the firmware via the UART, but am now looking to update in app from a web server similar to how it is done is the X-CUBE_GCPv2.
I actually have not tried it out yet, but looking at the code, I think the SBSFU in the X-Cube-GCP package is not the same as there are some things that are very different (like the slot names for example)
Need some advice from the ST reps here
Would it be easier to edit my current firmware to add in the web update capability or to Edit the sample X-CubeGCP project to "convert" it into my own project? Note the problem I usually have with sample projects is with changing the device family - so many ways to mess up here.